This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem writing to USB stick with TIVA launchpa



I am trying to interface a USB stick to TIVA launchpad and facing following problems:

1) The Disk is being recognized and enumerated ok.

2) The following code is being used to create a file and write any data to it. The file is created on the disk but with zero bytes.

 

int testfs (void)

{

    FRESULT fr;

    FIL fil;

UINT noofchar;

    /* Open or create a log file and ready to append */

    fr = open_append(&fil, "logfile.txt");

    if (fr != FR_OK) return 1;

    /* Write Any Data */

    f_write(&fil,0,0x400,&noofchar);

    f_close(&fil);

    return 0;

}

I am using FATFS and the drivers provided by TI.

The file is created with 0 bytes and code hangs in the f_write function. Upon debugging and suspending it is found to break at USBHCDPipeWrite and stuck in the while loop at line 1626.

Please suggest a solution.

If a working example of writing to a usb stick on TIVA/STELLARIS . can be provided, it will be most helpful. I also have an ek-232 board in addition to the launchpad.

Regards