Other Parts Discussed in Thread: HALCOGEN
Hi,
I wish to set VCLK3 to 80MHZ for use with the EMIF on RM48HDK. The crystal into PLL1 is 16Mhz, PLL1 is giving 320MHZ and I have set VCLK3 divider to 3 and enabled VCLK3 config button in the GCM page of HalCoGen V3.06.
The code produced in system.c is as follows:
systemREG2->VCLKACON1 = ((1U - 1U ) << 24U)
| (0U << 20U)
| (SYS_VCLK << 16U)
| ((1U - 1U ) << 8U)
| (0U << 4U)
| SYS_PLL2;
Because I have set the divider to 3, as per spnu503b.pdf, table 2-75 bit field 10-8 the actual ratio bit should be 2 (= divide 3)
Therefore I think there is a bug in the above generated code and it should read:
systemREG2->VCLKACON1 = ((1U - 1U ) << 24U)
| (0U << 20U)
| (SYS_VCLK << 16U)
| ((3U - 1U ) << 8U)
| (0U << 4U)
| SYS_PLL2;
Can anyone from TI please confirm.
Thanks
Stomp!.