Hey... I have downloaded and installed VirtualBox and sucessfully got WIndows XP up and running on it.
Im on a Macbook Air .... and I am new to it also... so I am in the land of being at the mercy of internet help
Even worse, Im a uni student... so everyone here has an opinion which differs from everyone elses... and none of them have what I have...
I have XP running... I have I think been able to share the USB port... I have not installed drivers, but whenever I attempt to connect the stellaris to the XP virtualbox... it tells me its already in use...
is there a step by step do this for newbies? seriously, if windows were the only operating in the world, we would all be brainwashed... I thought I would give the mac a go... and I am putting on a UBUNTU partition also...
There really should be an easier way to depart windows...