This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

supported ARM processor for the applications



hi all

 plz help me out in choosing a ARM based TI Product fpr  ARM Based {Processor/Controler for the below applications

The following Programs are to be implemented on ARM Processor
1. Simple Assembly Program for
a. Addition | Subtraction | Multiplication | Division
b. Operating Modes, System Calls and Interrupts
c. Loops, Branches
2. Write an Assembly programs to configure and control General Purpose Input/Output (GPIO)
port pins.
3. Write an Assembly programs to read digital values from external peripherals and execute
them with the Target board.
4. Program for reading and writing of a file
5. Program to demonstrate Time delay program using built in Timer / Counter feature on IDE
environment
6. Program to demonstrates a simple interrupt handler and setting up a timer
7. Program demonstrates setting up interrupt handlers. Press button to generate an interrupt
and trace the program flow with debug terminal.
8. Program to Interface 8 Bit LED and Switch Interface
9. Program to implement Buzzer Interface on IDE environment
10. Program to Displaying a message in a 2 line x 16 Characters LCD display and verify the
result in debug terminal.
11. Program to demonstrate I2C Interface on IDE environment
12. Program to demonstrate I2C Interface – Serial EEPROM
13. Demonstration of Serial communication. Transmission from Kit and reception from PC using
Serial Port on IDE environment use debug terminal to trace the program.
14. Generation of PWM Signal
15. Program to demonstrate SD-MMC Card Interface.
Part -II:
Write the following programs to understand the use of RTOS with ARM Processor on IDE
Environment using ARM Tool chain and Library:
1. Create an application that creates two tasks that wait on a timer whilst the main task loops.
2. Write an application that creates a task which is scheduled when a button is pressed, which
illustrates the use of an event set between an ISR and a task
3. Write an application that Demonstrates the interruptible ISRs(Requires timer to have higher
priority than external interrupt button)
4. a).Write an application to Test message queues and memory blocks.
b).Write an application to Test byte queues
5. Write an application that creates two tasks of the same priority and sets the time slice period
to illustrate time slicing.
Interfacing Programs:
6. Write an application that creates a two task to Blinking two different LEDs at different timings
7. Write an application that creates a two task displaying two different messages in LCD display
in two lines.
8. Sending messages to mailbox by one task and reading the message from mailbox by another
task.
9. Sending message to PC through serial port by three different tasks on priority Basis.
10. Basic Audio Processing on IDE environment.