Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hi,
I'm working with a RM48L952 using the development board TMDXRM48HDK.
I've used the HET1 module to switch the LEDs on/off wich works pretty fine. Today I've seen that the HET1 module is not selected in the PINMUX-Section in HALCoGen(nothing is selected in PINMUX at all) they are only set as output pin in HALCoGen in HET1->Pin x-y.
5 of the 8 LEDs are using the HET-Pins 17, 25, 27, 29 and 31 who are not muxed to the chips outputs by default.
My question is why those LEDs are working when they are not selected to get muxed?