Other Parts Discussed in Thread: LM3S817
Hi,
We are using 3-phase AC induction motor for solar systems. For this we are using LM3S817 micro controller. we developed the code for 3-phase induction motor using redsuite3.0 IDE. When we are generating the sinewave 80% is the maximum dutyfunction we are getting at 50Hz. Is there any limitation for that or it is only the maximum. please provide the solution to get the 100% dutyfunction at 50Hz.