Other Parts Discussed in Thread: TM4C123GH6PM
Hello everybody,
I'm using the TM4C123GH6PM together with TivaWare code and I'm getting a strange linker warning:
Description Resource Path Location Type
#10247-D creating output section "vtable" without a SECTIONS My_stack_project C/C++ Problem
I find this weird because I have my lm4f230h5qr.cmd in the project and it's also selected in the project properties. The contents of the lm4f230h5qr.cmd file is this:
/******************************************************************************
*
* Default Linker Command file for the Texas Instruments LM4F230H5QR
*
* This is part of revision 9385 of the Stellaris Peripheral Driver Library.
*
*****************************************************************************/
--retain=g_pfnVectors
MEMORY
{
FLASH (RX) : origin = 0x00000000, length = 0x00040000
SRAM (RWX) : origin = 0x20000000, length = 0x00008000
}
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M4_T_le_eabi.lib */
/* Section allocation in memory */
SECTIONS
{
.intvecs: > 0x00000000
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.vtable : > 0x20000000
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
}
__STACK_TOP = __stack + 256;
Any idea how might I get rid of this warning? Thanks