This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the bootloader for LM4F232H5QR

HI:

     now I want to use the SD card to update the app code .

     I creat the project. then do:

1.   copy the "boot_loader"   to the project.(the "boot_loader"  come from "StellarisWare".)

2.  delete some update files which i do not use (e.g.: bl_can.c;bl_uart.c;)

3.  In "bl_config.h", I enable the BL_HW_INIT_FN_HOOK,and define the "SD_ENABLE_UPDATE"

      “#define BL_HW_INIT_FN_HOOK      MyHwInitFunc”

      “#define   SD_ENABLE_UPDATE” 

4.  creat bl_hooks.c file ,and add it into boot_loader folder.

      bl_hooks.c :

       #include "bl_hooks.h" 

        #include "bl_config.h"  

          #include "bsp.h"          /* the head file for the system driver*/

         void MyHwInitFunc(void)

         {  

                  BSP_Init();             //  the driver for spi, gpio, and so on

        }

5. then I add a interrupt  in the “bl_startup_ccs.s”:

      .if $$defined(ENET_ENABLE_UPDATE)

              .ref    SysTickIntHandler

               .word   SysTickIntHandler               ;; Offset 3C: SysTick handler

      .else

              .if $$defined(SD_ENABLE_UPDATE)    ; it is enable in the bl_config.h

                     .ref   Tmr_TickISR_Handler            ; have define in bps.c

                    .word  Tmr_TickISR_Handler

               .else

                       .word   IntDefaultHandler               ;; Offset 3C: SysTick handler

               .endif

    .endif

6. creat the BPS folder, which include the system initialize c files

7.  creat the driver folder, which include the LCD drivers.

8.  add FATFS file system.

then I build, the "console" displays:

<Linking>

This application has requested the Runtime to terminate it in an unusual way.
Please contact the application's support team for more information.
warning #10278-D: LOAD placement specified for section
   ".text:decompress:none:rtsv7M4_T_le_v4SPD16_eabi.lib<copy_decompress_none.ob
   j>". This section contains decompression routines required for linker
   generated copy tables and C/C++ auto-initialization.  Must ensure that this
   section is copied to run address before the C/C++ boot code is executed or
   is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section
   ".text:rtsv7M4_T_le_v4SPD16_eabi.lib<memcpy_t2.obj>". This section contains
   decompression routines required for linker generated copy tables and C/C++
   auto-initialization.  Must ensure that this section is copied to run address
   before the C/C++ boot code is executed or is placed with single allocation
   specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section
   ".text:decompress:ZI:rtsv7M4_T_le_v4SPD16_eabi.lib<copy_zero_init.obj>".
   This section contains decompression routines required for linker generated
   copy tables and C/C++ auto-initialization.  Must ensure that this section is
   copied to run address before the C/C++ boot code is executed or is placed
   with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section
   ".text:decompress:rle24:rtsv7M4_T_le_v4SPD16_eabi.lib<copy_decompress_rle.ob
   j>". This section contains decompression routines required for linker
   generated copy tables and C/C++ auto-initialization.  Must ensure that this
   section is copied to run address before the C/C++ boot code is executed or
   is placed with single allocation specifier (ex. "> MEMORY").
warning #10278-D: LOAD placement specified for section
   ".text:rtsv7M4_T_le_v4SPD16_eabi.lib<copy_decompress_rle.obj>". This section
   contains decompression routines required for linker generated copy tables
   and C/C++ auto-initialization.  Must ensure that this section is copied to
   run address before the C/C++ boot code is executed or is placed with single
   allocation specifier (ex. "> MEMORY").
table.c:4070:internal fatal error #10220: (".data:mmc-lm4f231e5qr.obj")

INTERNAL ERROR: D:\ti\ccsv5\tools\compiler\tms470\bin\lnk470.exe aborted


This is a serious problem.  Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.


>> Compilation failure
gmake: *** [sd_bootload.out] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****

My IDE is CCS5.1, and boot_loader copy from "StellarisWare"

Today, I download the CCS5.4, and copy the boot_loader form "TivaWare_C_Series-1.1", the same problem.

please help me , i will be mad.

1856.sd_bootload.rar