This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem about CCS used for TMS570LS3137

Hi ,all

    I use CCSV5.3 to develop code,When I enable safety function and RTI module ,I find the nERROR pin is low .And at last ,I found in sys_startup.c the code "__TI_auto_init();" caused the problem. If I delete this ,the problem disappear.I want to know what this  __TI_auto_init(); does ,why it caused the nERROR pin low .

 

  • Hi Jiaming,

    TI_auto_init() is a function which is used to initialize the copy table.

    Can you pls attach the project, so that we can have a look at it to understand the error.

  • (TMS570LC43, CCS55, FreeRtos)

    Hello, I have a problem with  TI_auto_init(), it doesn't work.

    I have to use the old fashion code and also, have to change something cause I've got null pointer and I have to skip it (refer to count++ below).

    It seems not to be always the case, sometimes for a build it's ok, I don't know why.

    extern "C" void copy_in( void *binit );

    extern "C" void __TI_auto_init( void );

    extern "C" void _c_int00();

    /**** CODE TEMPORAIRE POUR PATCH GLOBAL_INIT **/

    //// Type Definitions

    typedef void (*handler_fptr)(const unsigned char *in, unsigned char *out);

    // External flags

    extern unsigned long * __binit__;

    extern unsigned long   __TI_Handler_Table_Base;

    extern unsigned long   __TI_Handler_Table_Limit;

    extern unsigned long   __TI_CINIT_Base;

    extern unsigned long   __TI_CINIT_Limit;

    extern unsigned long  __TI_INIT_ARRAY_Base;

    extern unsigned long  __TI_INIT_ARRAY_Limit;

    /**********/

    extern short _RamfuncsLoadStart;

    extern short _RamfuncsLoadEnd;

    extern short _RamfuncsRunStart;

    volatile unsigned long countRam = 0;

    #pragma CODE_STATE(32)

    void CopyRamFuncs( void )

    {

      short *src  = &_RamfuncsLoadStart;

      short *end  = &_RamfuncsLoadEnd;

      short *dest = &_RamfuncsRunStart;

      while( src < end )

      {

         *dest = *src;

         dest++;

         src++;

         countRam++;

      }

    }

    #pragma CODE_STATE(32)

    #pragma INTERRUPT(RESET)

    void _c_int00()

    {

      switch( DrvSys::GetResetSource() )

      {

         case DrvSys::POWERON_RESET:

         case DrvSys::EXT_RESET:

         case DrvSys::OSC_FAILURE_RESET:

         case DrvSys::WATCHDOG_RESET:

         case DrvSys::CPU0_RESET:

         case DrvSys::CPU1_RESET:

         case DrvSys::SW_RESET:

         default:

            // Disable cache during initialization

            CoreDisableCache();

            // Enable floating point unit

            CoreEnableVfp();

            // Initialize L2RAM to avoid ECC errors right after power on

            MemoryInit();

         case DrvSys::DEBUG_RESET:

         case DrvSys::NO_RESET:

            // When no reset or debug reset, do not reinitialize memory to allow passing values

            // between programs

            CoreDisableCache();

            // Clear reset source

            DrvSys::ClearAllResetSource();

            // Initialize Core Registers to avoid CCM Error

            CoreInitRegisters();

            // Initialize Stack Pointers

            CoreInitFiqStackPointer( FIQ_STACK_ADDR );

            CoreInitIrqStackPointer( IRQ_STACK_ADDR );

            CoreInitAbortStackPointer( ABORT_STACK_ADDR );

            CoreInitUndefStackPointer( UNDEF_STACK_ADDR );

            CoreInitUserStackPointer( USER_STACK_ADDR );

            CoreInitSvcStackPointer( SVC_STACK_ADDR );

            // Enable CPU Event Export

            // This allows the CPU to signal any single-bit or double-bit errors detected

            // by its ECC logic for accesses to program flash or data RAM.

            CoreEnableEventBusExport();

            // Copy RAM functions to RAM.

            CopyRamFuncs();

            // Initialize System - Clock, Flash settings with Efuse self check

            DrvSys::Init( DrvSys::OSC_16MHZ_PLL_300MHZ );

            // Initialize all peripherals in safe mode

            DrvInit::SafeInit();

            // Enable IRQ offset via VIC controller

            CoreEnableIrqVicOffset();

            // Disable Error signal module and clear errors

            DrvEsm::Init();

            // Initialize VIM table

            DrvVim::Init();

            // initialize global variable and constructors

            //__TI_auto_init();

    /**** CODE TEMPORAIRE POUR PATCH GLOBAL_INIT **/

            //// Initialize copy table

            if( (unsigned *)&__binit__ != (unsigned *)0xFFFFFFFF )

            {

               copy_in( (void *)&__binit__ );

            }

            // Initialize global variables

            typedef void (*handler_fptr)(const unsigned char *in, unsigned char *out);

            if( &__TI_Handler_Table_Base < &__TI_Handler_Table_Limit )

            {

               unsigned char **tablePtr   = (unsigned char **)&__TI_CINIT_Base;

               unsigned char **tableLimit = (unsigned char **)&__TI_CINIT_Limit;

               while( tablePtr < tableLimit )

               {

                  unsigned char *loadAdr = *tablePtr++;

                  unsigned char *runAdr  = *tablePtr++;

                  unsigned char  idx     = *loadAdr++;

                  handler_fptr   handler = (handler_fptr)(&__TI_Handler_Table_Base)[idx];

                  (*handler)( (const unsigned char *)loadAdr, runAdr );

               }

            }

            // Initialize Constructors

            typedef void (**DFPtr)(void);

            void (**base)() = (DFPtr)&__TI_INIT_ARRAY_Base;

            void (**limit)() = (DFPtr)&__TI_INIT_ARRAY_Limit;

            volatile unsigned long count = 0;

            while( base < limit )

            {

               void (*p)() = *base++;

               if(*p != 0)

               {

                  p();

               }

               else

               {

                  count++;

               }

            }

    /*****************************/

            // Call the application

            RunMain();

            break;

      }

      //Exit();