Other Parts Discussed in Thread: RM48L952, HALCOGEN, RM48L950
Hello
I am using the RM48L952 at 220MHz, Silicon Revision B and HalCoGen 3.6.0.
In Halcogen it is not possible to configure the Flash wait states to 3. If I enter 3 and set the focus to another GUI element, Halcogen corrects the value back to 4.
I am aware that in silicon revision A an entry in the errata-sheet required to configure 4 waitstates. However, the current errata sheet does not list that bug anymore.
Am I right, that this is a HalCoGen bug? Or is it still necessary to configure 4 wait-states at 220MHz?
Best regards,
Flurin