Other Parts Discussed in Thread: UNIFLASH
Hi everybody.
When I try to debug an example code with CCS V5.5 and flash the Hercules development kit, this error message appeared :
"IcePick: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.1.232.0) "
I think it's a problem with the XDS100V2 driver, it's doesn't seems to be installed... (it's doesn't appeared in my USB peripherals).
How can I solve this ?
Thanks !