Other Parts Discussed in Thread: RM48L952, HALCOGEN
We are using a TMDXRM48HDK in our current project to evaluate the possibilities of the RM48l952 as long as our Hardware-Team is working on our schematics.
Yesterday i wanted to test the ADC and after activating the ADC in HALCoGen i connected a potentiometer (1kOhm) to ADC-Pin8:
GND to J11[79]
VCC to 5V(TP23)
the middle pin to J9[51](says AD1IN 8)
the moment i plugged in the pin to the ADC-chanel the RM84 got hot as hell (nearly burned my finger). I unplugged USB and DC immediately, unplugged the potentiometer.
The RM48 is still working (a sci-send-loop is still sending) but i can't connect to the programmer via USB and the chip still gots very hot(not as hot as before but hotter than normal).
I checked the RM48 datasheet (SPNS177B) and section 3.1says that the input voltage for all ADC pins is -0.3V to 5.5V
Is there any possibility to save the board and where i made the mistake?