Other Parts Discussed in Thread: TM4C123GH6PZ
Dear all, the mcu in my custom board is TM4C123H6PZI, the emulator is XDS100V3, the problem is:
When the mcu's flash is empty, no matter using "Lm flash programmer" through mcu's UART0 or using the emulator, the firmware image can be programmed into the mcu's flash successfully; but when the mcu's flash is not empty,no matter using "Lm flash programmer" through mcu's UART0 or using the emulator,the firmware image cann't be programmed into the mcu's flash . I doubt if the mcu's flash could be programmed only once or was protected by routines. Can anyone help me?
regards,
Rolan