Other Parts Discussed in Thread: TMS570LS20216, HALCOGEN
Dear TI Support:
I use TMS570LS20216 USB Kit and HallCoGen3.06.00 do the clock test. Here is my HallCoGen configuration:
I use main oscillator for the RTI model's clock source, on the usb kit, it's a 16MHz crystal.
And this is my RTI configuration:
I use block0 and block1 to generate compare0 and compare3 interrupts, the period of this two interrupts is 1ms and 10ms. In the interrupt notificaiton, flash the LEDs.
But the problem is : watch the LED flash frequency, it seems the actual period is about 4 times longer (4ms and 40ms), please tell me why.
Regards,
Node