This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GXL LMFLASH unlock problem



Hello, i have CCS5.5.000. yesterday i played a little bit with the sysclk. I changed the sysclock from 16MHz to 80Mhz.

And later the debug port was locked i dont know why. Now i can unlock the debug port with the LMFLASH, but if i power cycle the board it is locked again. And if i try to connect the locked board the CCS came with the error "Error to connecting to the target" If i press Cancel an other window with Error to connecting to the target and if i press OK CCS crashes. Any ideas?

Best regards

Franz

code:

int main(void) {
    uint32_t tmp;
    uint32_t pui32DataRx[3];
    uint32_t pui32DataTx[3];
//    uint8_t string[50];
//    tmp = 0;
    //
    // Enable lazy stacking for interrupt handlers.  This allows floating-point
    // instructions to be used within interrupt handlers, but at the expense of
    // extra stack usage.
    //
    ROM_FPUEnable ();
    ROM_FPULazyStackingEnable ();

    // Set the clocking to run directly from the crystal.
    ROM_SysCtlClockSet (SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | /*SYSCTL_USE_PLL |*/SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
//    SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);
// Enable the GPIO port that is used for the on-board LED.
    ROM_SysCtlPeripheralEnable (SYSCTL_PERIPH_GPIOF);
    // Enable the GPIO pins for the LED (PF2).
    ROM_GPIOPinTypeGPIOOutput (GPIO_PORTF_BASE, GPIO_PIN_2);
    // Enable the peripherals used by this example.
    ROM_SysCtlPeripheralEnable (SYSCTL_PERIPH_UART0);
    ROM_SysCtlPeripheralEnable (SYSCTL_PERIPH_GPIOA);

// set GPIO F4 for input button S1
    ROM_GPIOPinTypeGPIOInput (GPIO_PORTF_BASE, GPIO_PIN_4);
    ROM_GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_4, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);

    // Set GPIO A0 and A1 as UART pins.
    ROM_GPIOPinConfigure (GPIO_PA0_U0RX);
    ROM_GPIOPinConfigure (GPIO_PA1_U0TX);
    ROM_GPIOPinTypeUART (GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
    //
    // Configure the UART for 115,200, 8-N-1 operation.
    //
    //
    // Initialize the UART for console I/O.
    //
    UARTStdioConfig(0, 115200, SysCtlClockGet());
    UARTFIFOEnable(UART0_BASE);

//    ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 115200,
//                            (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
//                             UART_CONFIG_PAR_NONE));
    //
    // Enable the UART interrupt.
    //
    ROM_IntEnable (INT_UART0);
    ROM_UARTIntEnable (UART0_BASE, UART_INT_RX | UART_INT_RT);
    //
    // Prompt for text to be entered.
    //
//    UARTSend((uint8_t *)"\033[2JEnter text: ", 16);
    UARTSend((uint8_t *) "FLOWSONIX LASER TEST\n\r", 22);
    UARTSend((uint8_t *) "--------------------\n\r", 22);
//    UARTSend((uint8_t *) "  Type: Single Ended\n\r", 22);
//    UARTSend((uint8_t *) "  Samples: One\n\r", 16);
//    UARTSend((uint8_t *) "  Update Rate: 250ms\n\r", 22);
    UARTSend((uint8_t *) "X=PE3 Y=PE2\n\r\n\r", 13);

//EEPROM
    ROM_SysCtlPeripheralEnable (SYSCTL_PERIPH_EEPROM0);
//    tmp = ROM_EEPROMSizeGet ();        // ok
//    UARTprintf("eeprom_size:%04d\r\n", tmp);
    ROM_EEPROMRead (&PSD_ref_position[0], 4, 4);
    UARTprintf("Saved zero X:%04d\t", PSD_ref_position[0]);
    ROM_EEPROMRead (&PSD_ref_position[1], 8, 4);
    UARTprintf("Y:%04d,\r\n\r\n", PSD_ref_position[1]);
    tmp = SysCtlClockGet();

    //SPI
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    GPIOPinConfigure(GPIO_PA2_SSI0CLK);
//    GPIOPinConfigure(GPIO_PA3_SSI0FSS);
    ROM_GPIOPinTypeGPIOOutput (GPIO_PORTA_BASE, GPIO_PIN_3);    // A3 = output
    GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
    GPIOPinConfigure(GPIO_PA4_SSI0RX);
    GPIOPinConfigure(GPIO_PA5_SSI0TX);
    GPIOPinTypeSSI(GPIO_PORTA_BASE,
            GPIO_PIN_5 | GPIO_PIN_4 /*| GPIO_PIN_3*/| GPIO_PIN_2);
    SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 1000000, 8);
    SSIEnable(SSI0_BASE);
    // Read any residual data from the SSI port.  This makes sure the receive
    // FIFOs are empty, so we don't read any unwanted junk.  This is done here
    // because the SPI SSI mode is full-duplex, which allows you to send and
    // receive at the same time.  The SSIDataGetNonBlocking function returns
    // "true" when data was returned, and "false" when no data was returned.
    // The "non-blocking" function checks if there is any data in the receive
    // FIFO and does not "hang" if there isn't.
    //
    while (SSIDataGetNonBlocking(SSI0_BASE, &pui32DataRx[0])) {
    }
    pui32DataTx[0] = 0x5555;    //max 16bit
    pui32DataTx[1] = 0xAAAA;
    pui32DataTx[2] = 0;

    //
    // The ADC0 peripheral must be enabled for use.
    //
//    tmp = SysCtlPeripheralPresent(SYSCTL_PERIPH_ADC0);
    ROM_SysCtlPeripheralEnable (SYSCTL_PERIPH_ADC1);

    //
    // For this example ADC0 is used with AIN0 on port PE3.
    // The actual port and pins used may be different on your part, consult
    // the data sheet for more information.  GPIO port E needs to be enabled
    // so these pins can be used.
    // TODO: change this to whichever GPIO port you are using.
    //
    ROM_SysCtlPeripheralEnable (SYSCTL_PERIPH_GPIOE);

    //
    // Select the analog ADC function for these pins.
    // Consult the data sheet to see which functions are allocated per pin.
    // TODO: change this to select the port/pin you are using.
    //
    ROM_GPIOPinTypeADC (GPIO_PORTE_BASE, GPIO_PIN_3);    //AIN0
    ROM_GPIOPinTypeADC (GPIO_PORTE_BASE, GPIO_PIN_2);    //AIN1

    //
    // Enable sample sequence 3 with a processor signal trigger.  Sequence 3
    // will do a single sample when the processor sends a signal to start the
    // conversion.  Each ADC module has 4 programmable sequences, sequence 0
    // to sequence 3.  This example is arbitrarily using sequence 3.
    //
    ADCSequenceConfigure (ADC1_BASE, 0, ADC_TRIGGER_PROCESSOR, 0);

    //
    // Configure step 0 on sequence 3.  Sample channel 0 (ADC_CTL_CH0) in
    // single-ended mode (default) and configure the interrupt flag
    // (ADC_CTL_IE) to be set when the sample is done.  Tell the ADC logic
    // that this is the last conversion on sequence 3 (ADC_CTL_END).  Sequence
    // 3 has only one programmable step.  Sequence 1 and 2 have 4 steps, and
    // sequence 0 has 8 programmable steps.  Since we are only doing a single
    // conversion using sequence 3 we will only configure step 0.  For more
    // information on the ADC sequences and steps, reference the datasheet.
    //
    ROM_ADCSequenceStepConfigure (ADC1_BASE, 0, 0, ADC_CTL_CH0); //| ADC_CTL_IE );
    ROM_ADCSequenceStepConfigure (ADC1_BASE, 0, 1, ADC_CTL_CH1 | ADC_CTL_IE | ADC_CTL_END);

    //
    // Since sample sequence 3 is now configured, it must be enabled.
    //
    ROM_ADCSequenceEnable (ADC1_BASE, 0);

    // Clear the interrupt status flag.  This is done to make sure the interrupt flag is cleared before we sample.
    ROM_ADCIntClear (ADC1_BASE, 0);

    g_ui32Counter = 0;
    // Set up the period for the SysTick timer.  The SysTick timer period will
    // be equal to the system clock, resulting in a period of 1 second.
    tmp = SysCtlClockGet();
    SysTickPeriodSet(SysCtlClockGet() / 8); // SysCtlClockGet == 16Mhz
    SysTickIntEnable();        // Enable the SysTick Interrupt.
    SysTickEnable();        // Enable SysTick.

    //
    // Enable processor interrupts.
    //
    ROM_IntMasterEnable ();
    LCD_init();
    LCD_print(" --FLOWSONIX TEST-- ");

    while (1)        // Loop forever echoing data through the UART.
    {
        ROM_ADCProcessorTrigger (ADC1_BASE, 0);// Trigger the ADC conversion.
        while (!ADCIntStatus(ADC1_BASE, 0, false)) { }// Wait for conversion to be completed.
        ROM_ADCIntClear (ADC1_BASE, 0);// Clear the ADC interrupt flag.
        ROM_ADCSequenceDataGet (ADC1_BASE, 0, pui32ADC0Value);// Read ADC Value.
//        ADCSequenceDataGet(ADC0_BASE, 1, &pui32ADC0Value[1]);

        //
        // Display the AIN0 (PE7) digital value on the console.
        //
//        UARTprintf("AIN0=%04d   AIN1=%04d\r\n", pui32ADC0Value[0],pui32ADC0Value[1]);
        UARTprintf("%04d,\t%04d\r\n", pui32ADC0Value[0], pui32ADC0Value[1]);
//        UARTprintf("printf\t");

        //       SSIDataPut(SSI0_BASE, pui32DataTx[0]);
        //       SSIDataPut(SSI0_BASE, pui32DataTx[1]);

        //
        // Wait until SSI0 is done transferring all the data in the transmit FIFO.
        //
//        while(SSIBusy(SSI0_BASE))
//        {
//        }
//        SSIDataGet(SSI0_BASE, &pui32DataRx[0]);
//        tmp = GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_4);
        static unsigned char button_save;
        if (!(GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_4) == GPIO_PIN_4)) {
            ROM_SysCtlDelay (SysCtlClockGet() / (3 * 100)); // 100=10ms delay
            if ((!(GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_4) == GPIO_PIN_4))
                    && !button_save) {
                button_save = true;
                UARTprintf("---Save to EEPROM X:%04d Y:%04d\r\n",pui32ADC0Value[0], pui32ADC0Value[1]);
                while(ROM_EEPROMStatusGet());
                tmp = ROM_EEPROMProgramNonBlocking(pui32ADC0Value[0],4);
                while(ROM_EEPROMStatusGet());
                tmp = ROM_EEPROMProgramNonBlocking(pui32ADC0Value[1],8);
                LCD_f(C_LINE_4);
                LCD_print("zero Position saved");
                ROM_SysCtlDelay (SysCtlClockGet() / (3 * 1)); // 1=1sec. 2=0,5sec.
                LCD_f(C_LINE_4);
                LCD_print("                    ");
            }
        }
        else
        {
            button_save = false;
        }
        LCD_f(C_LINE_2);
        usprintf(lcd_string, "Cnt:%d", systickcounter);
        LCD_print(lcd_string);
        LCD_f(C_LINE_3);
        usprintf(lcd_string, "  X:%04d    Y:%04d", pui32ADC0Value[0], pui32ADC0Value[1]);
        LCD_print(lcd_string);

        // This function provides a means of generating a constant length // delay.  The function delay (in cycles) = 3 * parameter.  Delay
        // 250ms arbitrarily.
        ROM_SysCtlDelay (SysCtlClockGet() / (3 * 10)); // 1=1sec. 2=0,5sec.
    }
}

  • Hello, with an other project it is working.

    Is it possible to brick the ADC with the setting

    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);

    I have problems with the adc. at this line i get FaultISR. What is happening?

        // Set the analog mux value for this step.
        HWREG(ui32Base + ADC_SSMUX) = ((HWREG(ui32Base + ADC_SSMUX) &
                                        ~(0x0000000f << ui32Step)) |
                                       ((ui32Config & 0x0f) << ui32Step));


  • Hello, i have played around with the bord and it is working again.?!?

    What i have done is to add while(ROM_EEPROMStatusGet());

    after switching on the EEPROM CLK.

    ROM_SysCtlPeripheralEnable (SYSCTL_PERIPH_EEPROM0);

    maybe the EEPROM was not ready for reading?

     

  • Using SYCCTL_SYSDIV_1 in the following call is not correct. The system clock has be less or equal than 80MHz for the part, the following call is to set the clock to be 200MHz which is not valid.

     SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);

    You can get 16MHz by using SYSCTL_SYSDIV_12 instead. Try that, and see if the problem goes away.

    Angela

  • @ Angela,

    Your identification of  poster's 200MHz improper/unwanted "creation" is applauded.  Suspect though that,   "SYSCTL_SYSDIV_12" likely yields 200/12 = 16.666MHz - and our belief is that "16MHz or above" satisfies ADC's demand.

    @ Poster,

    Initial post weaves many functions - is substantial - thus complicates read/review by your, "helpers."  (offical or otherwise) 

    Might it better serve your purpose - both in your individual test/troubleshooting - and when posting here - to reduce your code to the minimum which illustrates your issue?

    Later - after each individual functional area has been tested/verified - you can enable all.  (more likely now to run w/out issue...)