Other Parts Discussed in Thread: RM48L952
Hi,
I have few questions for I/O output current of RM48L952.
These pins can drive 2mA, 4mA or 8mA current from datasheet of rm48l952.
Q1. How many amperes the pin can output with pull up to 3.3v? How many amperes the pins can output without pull up?
Q2. How many ohms the pull up and pull down resistor?
Q3. If I can increate the output current (for example 10mA ) by setup a pin's PDR to "1" , set its PSL to "0" with a external pull up resistor ?
If I do like this. Whether the output pin will be damaged by inspiratory current which is bigger the 2mA, 4mA or 8mA current ?
Thanks,
Chuan