Hi,
I have noticed that the VIM channel mapping is different now in v03.06.00 and it doesn't match VIM RAM, so what do I do if I wanna have gio interrupt triggered by falling edge? same as the old version?
v03.06.00
v03.05.02
Thank you
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have noticed that the VIM channel mapping is different now in v03.06.00 and it doesn't match VIM RAM, so what do I do if I wanna have gio interrupt triggered by falling edge? same as the old version?
v03.06.00
v03.05.02
Thank you
Kevin
Hi
They are absolutely same. From 3.05.02 to 3.06.00 we tired to strictly follow Data Sheets Naming convention. If you look at data sheet Interrupt "Request Assignment Table" you will only see GIO Interrupt A and GIO Interrupt B. Which actually corresponds to GIO High and Low Interrupts.