Hi,
I am trying to access Hercules Launchpad (Ref: http://www.ti.com/lit/ml/spnu587/spnu587.pdf) via Jlink, 20 pin, debugger. But IDE (KEIL UV4) can not detect RM42 DAP. I can see TCK & RTCK contains the clock, and TDI & TDO contains some data signals on Oscilloscope. Also, I can't find any document which describes usage of Hercules Launchpad via 14 pin JTAG.
I mounted connector J12 as referred by schematic and connected TI14 and ARM20 pins as follow.
TI 14 ARM 20
1 (TMS) 7 (TMS)
3 (TDI) 5 (TDI)
5 (PD) 1,2 (VREF)
7 (TDO) 13 (TDO)
9 (RTCK) 11 (RTCK)
11 (TCK) 9 (TCK)
13 (EMU0) No such signal
14 (EMU1) No such signal
2 (nTRST) 3 (nTRST)
No such signal 15 (nRST) with a pull up resistor (2.7K) to pin 1or 2 of ARM 20
4,8,10,12 (GND) 4,6,8,10,12,14,16,18,20 (GND)
Regards,
Vinod