Other Parts Discussed in Thread: TM4C123BH6PGE
Hi,
I developed my code using an EKLM4F120XL board and the ROM Bootloader (UART) was all working nicely. I have now ported the code onto my own board with a TM4C123BH6PGE and I can't get the ROM Bootloader working.
I have two methods of entering the Bootloader...
holding pin A6 low at power up, set up using this code...
//Set ForceBootloader Pin.......BOOTCFG..........................................................................................................
int regVal;
regVal = HWREG(0x400FE000 + 0x1D0); //read BOOTCFG
if(regVal & 0x00000100) { //check EN bit - if set, program BOOTCFG
HWREG(FLASH_CTRL_BASE + 0x00) = 0x75100000; //FMA addr
HWREG(FLASH_CTRL_BASE + 0x04) = 0x00001802; //FMD data PA6 pulled low - my board
//HWREG(FLASH_CTRL_BASE + 0x04) = 0x00003402; //FMD data PB5 pulled low - launchpad
HWREG(FLASH_CTRL_BASE + 0x08) = 0xA4420008; //FMC key | commit //key should be 71D5 no?
delayms(2); //wait for flash write
}
//regVal = HWREG(0x400FE000 + 0x1D0); //read BOOTCFG to test it was actually written
and entering the Bootloader from my code using this code...
void EnterBootloader(void)
{
ROM_IntMasterDisable(); //disable interrupts master
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOA); //get UART reset to simple, no interrupts, no handshake
ROM_GPIOPinConfigure(GPIO_PA0_U0RX); //set up pins PA0 and PA1 for UART use
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
ROM_UARTDisable(UART0_BASE); //disable while we set it up
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_UART0);
ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 38400, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
//ROM_UARTEnable(UART0_BASE); //flush rx buffer??
//while(ROM_UARTCharsAvail(UART0_BASE))
// ROM_UARTCharGet(UART0_BASE);
ROM_UpdateUART(); //will not return from here - needs hardware reset
}
Neither method is working for me - entering with the pin held low does appear to run some other code than mine, but the LMFlash Programmer does not connect. I am watching the tx and rx lines on a scope and there is no response from the Tiva to the LMFlash "hello". If I enter from my code it drops straight out and runs my code as if we had just reset.
Is anybody aware of a difference between the Stellaris and the Tiva here? The only difference on my board is that the main osc is 25MHz rather than 16Mhz on the Launchpad. The UART works fine in my code, so the hardware is OK.
Thanks in advance!
Richard