Other Parts Discussed in Thread: TMS570LS2134
Hi there,
Might be a dumb question ... on the PGE 144-pin package TMS570LS2134 MCU, the SPI4 and MibSPI5 each has only one single chip-select signal (CS0), and I need to use one of them to address two external SPI devices.
Can your expert tell me whether it is possible to add some glue logics to share the single CS0 line for two external SPI devices (i.e. CS0 connected to one device and /CS0 using external inverter connected to the other one)?
In other words, is it possible for the internal SPI4/MibSPI5 to clock in/out data when the CS0 signal is commanded to be HIGH while writing to the DAT0/DAT1 registers?
Thanks!