This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMI-Mode for output pins

Hi,

on our RM46L852ZWT I want to enable the output buffer low emi mode for all (but at least for the EMIF) output pins.

The register description (technical manual page 164) is not really clear to me. It seems that the low emi mode is enabled by clearing the corresponding bits.

I did it (I set bit 15..0 in the GPREG1 to 0x0000).

A direct comparison with a spectrum analyzer and a RF-current probe showed no difference.

Do I have to do something else to enable the EMI-mode?

Regards,

Markus