This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Automotive daughter board (CAN/LIN) for Hercules LaunchPad Serries

Hello,  

we're very interessting to use the hercules LaunchPad eval-board for lin and CAN applications.

Is there a kind of automotive daughter board for the "new" Hercues LaunchPad Series. 

Has perhaps even TI itself produced such a demo-example board ?

Kind regards. Thomas

 

  • I'm personally working on one ("community" built we'll call it) that should be a generic CAN boosterpack for all LaunchPads.

    See http://forum.43oh.com/topic/4202-can-boosterpack/

    The connectors on this board will be RJ45, intended for simple MCU-to-MCU comms, but I have a small adapter board to convert RJ45 to the DE9 pinout commonly used with OBD-II cables (also has an onboard buck converter to step 12VDC down to 5VDC).

  • We have not built such a demo-example board.

    Regards,

    Haixiao