Other Parts Discussed in Thread: HALCOGEN
Hi there,
I'm using RM46 and HalCoGen v3.5.2.
I' modulating the PLL1.
The user manual says, that "Multiplier Correction" (MULMOD) can be set from 0 to 511,
but I can change the value in HalCoGen (by clicking the small arrows!) only from 7 to 255.
Are the other values (e.g. '0' or '511') not allowed for MULMOD?
How is this value affecting the frequency of the PLL?
(The formular (5), page 373, NF= (PLLMUL + MULMOD+ 1<<8)/256
is a little bit confusing....)
Best regards,
Andy