Other Parts Discussed in Thread: TMS570LS20216, TMS570LS2134
Hi there,
In the spnu489c for the TMS570LS20216 MCU, page 194, Table 6-2 states that march13n_red algorithm number is 3 (or 0x00000004) for single-port memories, and the number is 4 (or 0x00000008) for two-port memories.
While in the spnu499a for the TMS570LS2134, page 118, Table 2-15 states that the reverse, that march13n_red algorithm number is 4 (or 0x00000008) for single-port memories, and the number is 3 (or 0x00000004) for two-port memories.
Can you tell whether this is as per the different MCU design or it is an error? If so, which one is right?
Thanks.