Other Parts Discussed in Thread: HALCOGEN
Hi,
I'm working with both ADC in a RM48 Hercules HDK. Setting the timing of both I'm experimenting this strange behaviour.
As you can see from the screenshot the Cycle time for both ADC is set to 35ns but while the tConversion for ADC1 group event is shown as 0.455us the same parameter for ADC2 is shown as the 1.3us. It seems that changing the VCLK1 prescale the parameter is not updated. Note that this behaviour is limited to the ADC2 Group event while all the other tConversion for both ADC are correctly updated.
The generated code for both ADC set the same registers at the same values.
Can I ignore this assuming is a HalCoGen MMI bug?