This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

N2HET, BR instruction: Difference of the events "ZERO" and "EQ, Z"

Hi.

My question is regarding the N2HET module, of the TMS570LS31x.

In spnu499b.pdf, page 852, in "Table 20-59. Branch Condition Encoding for BR", is stated

  • in line 5: "ZERO 1 0 0 0 0 If Zero flag is set"
  • in line 11: "EQ, Z 0 0 1 0 1 Equal or Zero: Z==1"

IMHO in both cases is checked if the Zero flag is set. So IMHO they are the same. But what is this good for?

If they are not the same, I would ask you to describe the difference between these two conditions.

Or is in line 11, in column "Branch Condition" something missing?

Regards

Oliver.