Other Parts Discussed in Thread: EK-TM4C123GXL
HI,
I'm trying to communicate the EK-TM4C123GXL with a bluetooth module through UART.
I take the uart_echo example and expand it to use UART0 to display info and UART4 to do the actual work.
I'm able to send command and get correct response to show up in the scope.
But the interrupt handler for UART4 seems to keep firing indefinitely. Here is part of my code:
//*****************************************************************************
//
// The UART interrupt handlers.
//
//*****************************************************************************
void
UARTIntHandler0(void)
{
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32Status = ROM_UARTIntStatus(UART0_BASE, true);
//
// Clear the asserted interrupts.
//
ROM_UARTIntClear(UART0_BASE, ui32Status);
//
// Loop while there are characters in the receive FIFO.
//
while(ROM_UARTCharsAvail(UART0_BASE))
{
//
// Read the next character from the UART and write it back to the UART.
//
char ch = ROM_UARTCharGetNonBlocking(UART0_BASE);
ROM_UARTCharPutNonBlocking(UART0_BASE, ch);
if (ch=='1') {
GPIOPinWrite(GPIO_PORTF_BASE, RED_LED|BLUE_LED|GREEN_LED, RED_LED);
}
else if (ch=='2') {
GPIOPinWrite(GPIO_PORTF_BASE, RED_LED|BLUE_LED|GREEN_LED, 0);
}
else if (ch=='3') {
//ble_cmd_system_hello();
UART4Send((uint8_t *)"\4\0\0\0\1",5);
//blink the LED
GPIOPinWrite(GPIO_PORTF_BASE, RED_LED|BLUE_LED|GREEN_LED, GREEN_LED);
SysCtlDelay(SysCtlClockGet() / (1000 * 3));
GPIOPinWrite(GPIO_PORTF_BASE, RED_LED|BLUE_LED|GREEN_LED, 0);
}
}
}
void
UARTIntHandler4(void)
{
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32Status = ROM_UARTIntStatus(UART4_BASE, true);
//
// Clear the asserted interrupts.
//
ROM_UARTIntClear(UART4_BASE, ui32Status);
// Show that some respnoses are received
UART0Send((uint8_t *)"h",1);
}
//*****************************************************************************
//
// This example demonstrates how to send a string of data to the UART.
//
//*****************************************************************************
int
main(void)
{
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
FPUEnable();
FPULazyStackingEnable();
//
// Set the clocking to run directly from the crystal.
//
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// Enable the GPIO port that is used for the on-board LED.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//
// Enable the GPIO pins for the LED (PF2).
//
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, RED_LED|BLUE_LED|GREEN_LED);
//
// Enable the peripherals used by this example.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART4);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
//
// Enable processor interrupts.
//
IntMasterEnable();
//
// Set GPIO A0 and A1 as UART pins.
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinConfigure(GPIO_PC4_U4RX);
GPIOPinConfigure(GPIO_PC5_U4TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_4 | GPIO_PIN_5);
//
// Configure the UART for 115,200, 8-N-1 operation.
//
UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
UARTConfigSetExpClk(UART4_BASE, ROM_SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
UARTFlowControlSet(UART4_BASE, UART_FLOWCONTROL_NONE);
//
// Enable the UART interrupt.
//
IntEnable(INT_UART0);
UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);
IntEnable(INT_UART4);
UARTIntEnable(UART4_BASE, UART_INT_RX | UART_INT_RT);
ROM_UARTEnable(UART4_BASE);
//
// Prompt for text to be entered.
//
UART0Send((uint8_t *)"\033[2JEnter text: ", 16);
//
// Loop forever echoing data through the UART.
//
while(1)
{
}
}
Thanks,