Other Parts Discussed in Thread: TMS570LS3137
Hi all,
I'd just like to confirm that with OVER0 = 1 the PBIST ROM will load the appropriate settings so that I can test all RAM with all relevant algorithms with one single call of PBIST?
Secondly can you explain what Return Data Select (RDS) means, I've searched through the TMR for the TMS570LS3137 but cant find any explanation as to what it means.
Finally, I see there are registers for storing the first errors address (FSRA0&1) and data (FSRD0&1) while the counter ( FSRC0&1) registers are incremented when an error occurs and decremented when an error is processed, is there anyway of recording the address and data while the errors are found/being processed?
cheers,
alan