Hello Tiva Team!
I'm currently trying to drive a series of LEDs with just the Tiva-C 123 Launchpad, and I was curious if it was possible (and safe) to tie together GPIOs to get higher current outputs. Currently I'm outputing 8mA but I would like to get up to 16mA. I see that Tiva-C can sink up to 18mA in certain circumstances however I need to be able to both source and sink 16mA. I have the LEDs connected using a charlieplexing scheme and am only turning on one LED at a time.
So my question is, can I tie togeth GPIOs to get higher current output? I've seen this done with MSP430, but want to check if the same can be done for Tiva-C. Are the GPIOs protected with CLDs? If possible to connect the two pins, are there any risks associated with doing this? (e.g. one goes high first and casues a short, blowing out a pin).
I checked the datasheet and past e2e posts and couldn't find a definite answer. All help is greatly appreciated!
Nate