This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC readings lower than expected

Hello,

My adc readings for the TM4C126GH6PM (with 3.3v vref) seem to be some percentage lower than what I should be getting. I'm also seeing other odd behavior. First, here is my init code for the adc and some code from where I read:

// Initialize the ADC
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_2);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ADCSequenceConfigure(ADC0_BASE, 2, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE, 2, 1, ADC_CTL_END | ADC_CTL_IE | ADC_CTL_CH1);
ADCIntEnable(ADC0_BASE, 2);
ADCIntClear(ADC0_BASE, 2);
ADCSequenceEnable(ADC0_BASE, 2);

uint32_t seq_buf[4] = {0};

ADCProcessorTrigger(ADC0_BASE, 2);
while(!ADCIntStatus(ADC0_BASE, 2, false));
ADCSequenceDataGet(ADC0_BASE, 2, seq_buf);
ADCIntClear(ADC0_BASE, 2);

return seq_buf[1];

As you can see I have two adc channels being configured in steps in sequence 2.

If i measure 1.5 volts at the adc input, i get about 1400 counts from the adc. With a 3.3v vref and 12 bit adc I should be getting about 1800 counts for 1.5 volts.

In my application, I take one adc sample every 250 ms. If I plot the data I get something that looks like a sawtooth pattern:

Could this be a timing issue? I tried adding large delays before reading from the adc and saw no change.

Thanks,

-Brandon

Edit: I previously stated that I saw a slight sawtooth pattern in my samples, but that is actually normal for my application. My setup was incorrect when I initially checked it.

  • MCU manual for our LX4F device (predecessor of yours) reveals ~500 max series, "analog source resistance."  Cannot find your characterization of your input voltage source.  (Rs is defined/detailed under electrical specs - manual rear)

    We find it helpful to initially apply mid-scale, stable, low impedance voltage source as ADC signal input.  Any signal variations - at this initial stage - complicate your analysis.  Also usually proves helpful to change to a 4 or 8 step sequence - locked to that same channel.  (this reveals any time instability - w/in your introduced signal or the ADC internal network) 

    There is some, "channel to channel" interaction - you may adjust the input levels of any other channels (or remove all of them) to see if this "contributes" to your perceived measurement error.

    As always - proper powering of Vdda (we employ a small ferrite bead & filter cap @ Vdda) and Vddgnd prove helpful... When scoped - Vdda should be proper & rock-stable...

  • That seems to be what tripped me up. The output resistances of our sources are much higher than 500 ohms. I did a quick test with a low resistance voltage divider and the adc was returning the correct values. We just have to stick some buffers in between. 

  • Thank you, Sir.  Jelly bean op-amps - wired as voltage followers - may well serve that purpose...