Other Parts Discussed in Thread: RM48L952, HALCOGEN
Today, I observed some problems with HalCoGen and RM48L952 with selftests enabled:
- Enable FMCBUS2 Error Check in HalCoGen: The function fmcBus2Check needs a power on reset to work properly
- Enable ESRAM ECC Check in HalCoGen: The function checkRAMECC has some bugs:
The following line in checkRAMECC is...
if(!(((tcram1REG->RAMERRSTATUS & 0x1U) == 0x1U) && ((tcram1REG->RAMERRSTATUS & 0x1U) == 0x1U)))
and should be
if(!(((tcram1REG->RAMERRSTATUS & 0x1U) == 0x1U) && ((tcram2REG->RAMERRSTATUS & 0x1U) == 0x1U)))
In the same function a short delay is needed in order to pass the RAM ECC selftest:
u32Cnt = 2;
while( u32Cnt > 0)
{
u32Cnt--;
}
/* Force a single bit error in both the banks */
tcramA1bitError ^= 1U;
tcramB1bitError ^= 1U;
Without the delay the selftest will always fail. A reason for this could be caching?!
Could you please check this and confirm me that issue?
Thanks.