This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I/O pin availability on xxx4 parts greater than on xxx5 or xxx7 parts

Hello,

Could somebody please explain why the summary data for the TMS570LSxxxx-PGE family says that the xxx4 parts have 64 GPIO pins whereas the xxx5 (Flexray) and xxx7 (Flexray and Ethernet) both have 58 pins.

The datasheets seem to show the same pin assignments and the IOMM does not affect the Flexray pins which would be the obvious answer.

I would be interested to see a complete list of the pins that are qualified as GPIO.

Thanks,
Richard