Other Parts Discussed in Thread: NOWECC, UNIFLASH
Hello,
After reading about the SECDED in flash, I have a question, accordingo to:
"The ECC values for all of the ATCM program memory space (flash banks 0 through 6) must be
programmed into the flash before SECDED is enabled. This can be done by generating the correct values
of the ECC with an external tool such as nowECC or may be generated by the programming tool"
This means I can't save a file to flash, or change it several times, during run time? Would it work if I disabled ECC?