Other Parts Discussed in Thread: EK-TM4C123GXL
I just tried simple blinking exercise on PORTB on the TIVA C Series Board.
Every pin on the port works except PB7 which does not turn up.
Code:
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
int main(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_4|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE,GPIO_PIN_7|GPIO_PIN_6);
while(1)
{
GPIOPinWrite(GPIO_PORTB_BASE,GPIO_PIN_7|GPIO_PIN_6,0xc0);
SysCtlDelay(200000);
GPIOPinWrite(GPIO_PORTB_BASE,GPIO_PIN_7|GPIO_PIN_6,0x00);
SysCtlDelay(200000);
}
}
When this code runs, PB6 starts blinking but PB7 does not even turn on once.
What might be the problem?
Is there any alternate function for this pin(PB7), which this pin gets configured to, at every power up?
Do I need to disable any such alternate function?
Or is there some fault in hardware?