Other Parts Discussed in Thread: HALCOGEN, CCSTUDIO
Question about gpio interrupts. Configured Halcogen and sys_main.c as follows for the LaunchPad:
- on the driver tab: enable GIO
- on the GIO tab: for BIT7, set rising edge and enable VIM, high priority
- on the VIM Channel 0-31 tab: enable 9 GIO int A, IRQ
- generate code
- in the CCStudio, in the sys_main.c main function, add these 3 lines
_enable_IRQ();
gioInit();
while(1); - set breakpoint in gio.c gioHighLevelInterrupt()
- also set breakpoint in notification.c at gioNotification()
- start debug and push the button
The stop at breakpoint will not occur. Why???