Other Parts Discussed in Thread: RM48L952
Hi,
I have RM48L952. I'm trying implementing max 100 ms iteration of cycle which starts by externa events and comunikate over sci.
One iteration consist:
1 - gather some data
2 - transmit over sci in blocking mode
3 - parse received packet on sci ( receive is in interrupt mode or dma)
4 - run cpu self test over all 24 regions
5 - wait for external event whitch start new iteration
Points 1 - 3 is certainly less then 50ms. And communication baudrate is 115200 Receive on sci missing some data regardless on mode of operation (interrupt or dma) and receive by polling mode is not an option because this violates 100ms maximum period of one cycle.
I think that in spu self test dma or receiveinterrupt don't work. Is that true? And possibly how can I this evade?
Thanks in advance,
Luděk Hezina