Hi.
My question is regarding the TMS570LS3137.
My question is already stated in the discussion http://e2e.ti.com/support/microcontrollers/hercules/f/312/p/304060/1060473.aspx, title "Blocking behavior in case more than one flag for an ESM channel exists.", "Posted by Oliver Gr??ndonner on Nov 19 2013 07:31 AM". See especially the note at the end of the posting, i.e.:
"... NOTE: These are only two examples. But the question regarding the blocking behavior raises for ALL ESM channels for which there are two or more flags for one and the same ESM channel."
So if already the above discussion was opened, why I open a new discussion? Cause in the above discussion only the behaviour of ESM Group1, Channel 2, DMA - MPU, was discussed. But as stated in the note above: I need this inforamation for ALL ESM channels. And in "Posted by Anthony F. Seely on Nov 20 2013 18:12 PM" (of the above linked discussion) is stated
"The MPU in the DMA is unique so I would not regard this as a general answer for all IPs on the device. They need to be asked on a case-by-case basis. ..."
So I would ask you to provide the blocking behaviour for ALL ESM channels for which there are two or more flags for one and the same ESM channel.
Thank you and regards
Oliver.