Hello,
My requirement is an MCU with 8 UARTs, USB & graphic controller features. If such controller doesn't exist, is there any solution in TI?
Thanks & Regards
Harsha
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My requirement is an MCU with 8 UARTs, USB & graphic controller features. If such controller doesn't exist, is there any solution in TI?
Thanks & Regards
Harsha
You'll have to check to see if 8 UARTs appear but otherwise, newly introduced TM4C129X appears best suited due to its in-built LCD Controller & external bus access. (bus - to manage your required display frame buffer)
A development kit which includes a color Lcd was (is) available. Note that the LCD Controller version forces the present incarnation of that MCU into a BGA package.
Thanks for the reply,
I have a few more queries:
1. Is this part available in India
2. What screen resolution can I expect with this controller?
Regards,
Harsha
I'm simple vendor client - just like you - thus you can use normal means to determine availability, pricing, support etc.
As stated - TM4C129X data manual (or even data summary) should quickly reveal, "number of UARTs."
Unclear as to your real meaning of, "UART use - at the same time." In non-uDMA usage - your program code most usually will access one UART at a time. Through use of the uDMA the UART tasks may run, "in the background" - yet I am uncertain as to the number of uDMA channels this new MCU provides.
Some investigation effort falls to you, as you - by far - best know (and benefit) from those needs/objectives...