Other Parts Discussed in Thread: RM46L430
Hi,
Our customer is designing their board with the device RM46L430
We would like to know if the below connection is allowed with the USB.
According to the details of "USB Function Controller Connectivity" the
manual (SPNU514A- Figure 32-96) says only series resistor and a bypass capacitor
should be connected to the "VBUS" pin.
And according to the datasheet we understood that the VBUS pin has a internal pulldown.
But, we think the internal resistor may not be precise and there might be drift in its value.
So as a solution we are planning to use an external pull-down resistor as shown below.
please let us know if it is good to use an external pull-down and series resistor like this.