Hello,
"The values of the IO Control registers are only writable if Init bit of CAN Control Register is Cleared." is written at "27.17.29 TIOC" and "27.17.30 RIOC" in TRM of TMS570LS1227. Is the description correct?
I tried to do this, but "Func", "Dir", "Out", "In" bits are not writable.
Could you teach me the correct flow to use CAN 2 and CAN3 pins as GIO?
Best Regards.