This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Undefined entry on enable CPU event bus

Hello,

Whenever the bootloader reaches the _coreEnableEventBusExport_ function it  marks the  instruction as an undefined entry.

Here's the code for it. There is nothing wrong with it. whenver I load a different example it works perfectly, but when I try another then it just goes to an undefined entry.

    .def     _coreEnableEventBusExport_
    .asmfunc

_coreEnableEventBusExport_

        mrc   p15, #0x00, r0,         c9, c12, #0x00
        orr   r0,  r0,    #0x10
        mcr   p15, #0x00, r0,         c9, c12, #0x00
        mrc   p15, #0x00, r0,         c9, c12, #0x00
        bx    lr

    .endasmfunc
  • Pablo,

    Out of context, it is difficult to see what could be wrong.

    So let me ask some questions.

    1] Does the Core register initialization done correctly?
    2] Does the Stack initialization done correctly?
    3] Within the _coreEnableEventBusExport_routine, can you check the value of LR and see if it is pointing to the return address.

    Could you share more of your code to see your bootloader structure?

  • Hello,

    Sorry for such a vague question, but after some time away from the PC I found out that there was an instruction missing. The uC went into system mode, when it should've gone into supervisor mode.

    I was able to fix it.

  • Pablo,

    That is a good news. Can you than close this thread?

  • I would like to ask another question before that.

    When I'm reading ESMSR3 to check for any grouo 3 errors, it goes into a data abort excpetion.

    My code:

        if (ESMReg->ESMSR3) { /*If this happens the system must not continue with the boot process*/
            while(1);
        }

    The generated asm:

    00000d50: E59FC168 LDR R12, $C$CON5
    
    00000d54: E59CC000 LDR R12, [R12]
    
    00000d58: E35C0000 CMP R12, #0 00000d5c:
    
    0A000000 BEQ $C$DW$L$bootAfterReset$37$E

    After instruction @0x00000D50 I check that R12 is loaded with the correct address (0xFFFFF520), but when it executes the instruction @0x00000D54 it generates an interruption.

    Also the value @0xFFFFF520 = 0x0, which indicates that no group 3 errors occurred.

    The uC is in supervisor mode M[5..0]=10011 of CPSR. About this error I really have no idea what's going on.

  • Found the error. Reading from 0x0FFFF520 instead of 0xFFFFF520