This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

24 MHz clock output

Hi all, i've an LM4f120H5QR, can I generate a 24 MHz clock? I'm trying to use AHB on PORTB, but i've nothing

  • Giuseppe Giancola1 said:
    I've nothing

    "I've nothing," is serious/related kin to always precise, "Does not Work!"  (and - provides little diagnostic value...)

    AHB - properly set-up/config'ed - indeed enables faster output gpio toggling.

    Some (slight) clarification of "nothing" surely assists...

  • hi! sorry for the previous post, here is the code, in the startup.ccs there is the function Commuta at the Timer0 Submitter A line.

    the result is portB 7 LOW

    #include "timer_config.h"
    #include "inc/hw_types.h"                                                                       
    #include "driverlib/comp.h"
    #include "inc/hw_gpio.h"                                                                      
    #include "driverlib/pin_map.h"                                                                  
    #include "inc/hw_ints.h"                                                                  
    #include "inc/hw_memmap.h"                                                                   
    #include "driverlib/sysctl.h"                                                                   
    #include "driverlib/interrupt.h"                                                           
    #include "driverlib/rom_map.h"                                                            
    #include "driverlib/gpio.h"                                                                 
    #include "driverlib/timer.h"                                                             
    #include "driverlib/adc.h"
    #include "driverlib/ssi.h"                                                                
    #include "math.h"
    
    #ifdef DEBUG
    
    void__error__(char *pcFilename, unsigned long ulLine) {
    }
    
    #endif
    
    void Commuta(void);
    
    unsigned long ulPeriod;
    
     int main(void) {
         SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
         PortFunctionInit();
         SysCtlGPIOAHBEnable(SYSCTL_PERIPH_GPIOB);
         GPIOPinTypeGPIOOutput(GPIO_PORTB_AHB_BASE, GPIO_PIN_5);                                               
         GPIOPinWrite(GPIO_PORTB_AHB_BASE, GPIO_PIN_5, 0);
         SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
         TimerConfigure(TIMER0_BASE, TIMER_CFG_32_BIT_PER);
         ulPeriod=(SysCtlClockGet()/20000000)/2;
         TimerLoadSet(TIMER0_BASE, TIMER_A, ulPeriod -1);
         IntEnable(INT_TIMER0A);
         TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
         IntMasterEnable();
    
         TimerEnable(TIMER0_BASE, TIMER_A);
    
    
    
        while (1) {                                                                              
    
        }
    
    }
    
     void Commuta(void){
         TimerIntClear(TIMER0_BASE, TIMER_A);
    
         if(!GPIOPinRead(GPIO_PORTB_AHB_BASE, GPIO_PIN_5))
         GPIOPinWrite(GPIO_PORTB_AHB_BASE, GPIO_PIN_5, GPIO_PIN_5);
         else
         GPIOPinWrite(GPIO_PORTB_AHB_BASE, GPIO_PIN_5, 0);
    
     }

    THANKS!

  • Thank you - my understanding is that the, "toggling speed-up" gained via the AHB bus is essentially confined to gpio operations.  Thus - if the gpio operations are, "controlled" by an MCU timer - much of this benefit may be eroded.  (lost)

    You may confirm the correctness of AHB bus operation by implementing, "back to back" gpio function calls - first setting then clearing one or several AHB port pins.  Perhaps best to measure & confirm that first - then see if that AHB speed gain is indeed, "held hostage" by some MCU peripheral...

    Note: you likely should first compare/contrast such "back to back" gpio output via AHB versus APB bus.

  • ok, i understand...maybe I could have the pin toggle  with the pwm feature enabled?

  • Giuseppe Giancola1 said:
    have the pin toggle  with the pwm feature enabled

    Now you've got the idea/spirit - but I'm uncertain if the required GPIOPinConfigure() & GPIOPinType() may "accept" the AHB bus.  (I do not know)

    Suggest you'll gain by first performing simple, "toggle" of GPIO Port/Pins w/bus @ APB. (i.e. do not start w/PWM implemented!)   Note/log these results.  (20 or so, "back to back" set/clear - and then loop - this code-block will persist sufficiently for your scope to capture/review.)  With this APB bus as a measured baseline - switch to AHB - we note a nice, "speed-up."

    Once implemented & confirmed - launch your PWM and see if that "AHB" advantage remains.  Would be of interest to others (& myself) to learn of your results...  Bon chance, mon ami.

  • ok, thanks, to set or clear a pin without the high level API, i shoud use the HWREG(....) function, right?

  • Here's what we used:  (just showing 1st 4 fnt. calls - we repeated 20+ times to "firm" scope view...)

       while (1)
        {
       
        HWREG(GPIO_PORTF_AHB_BASE + GPIO_O_DATA + (GPIO_PIN_4 << 2)) = GPIO_PIN_4;

        HWREG(GPIO_PORTF_AHB_BASE + GPIO_O_DATA + (GPIO_PIN_4 << 2)) = 0; 
       
        HWREG(GPIO_PORTF_AHB_BASE + GPIO_O_DATA + (GPIO_PIN_4 << 2)) = GPIO_PIN_4;

        HWREG(GPIO_PORTF_AHB_BASE + GPIO_O_DATA + (GPIO_PIN_4 << 2)) = 0; 

        }

    Perhaps care, effort merits your award of, Verified Answer tick - this or other responses made your behalf...

  • Do implement the APB version of that code first - so that you establish a, "performance baseline."  Improvement should be readily noted.

    Thank you et bon chance, mon ami...

  • cb1_mobile said:

    have the pin toggle  with the pwm feature enabled

    Now you've got the idea/spirit - but I'm uncertain if the required GPIOPinConfigure() & GPIOPinType() may "accept" the AHB bus.  (I do not know)

    [/quote]

    APIs like GPIOPinConfigure or GPIOPinType can work with the AHB bus as well. You have to specify GPIO_PORTx_AHB_BASE instead of GPIO_PORTx_BASE as the base address of the port.

    Regards,

    Shashank

  • Thanks, but in this  way I have a max frequency of 200 kHz on the output pin also with a divider by 2000000 on ulPeriod.

  • @ Shashank,

    Don't believe the use of AHB Bus was missed.  (quote confirms)

    While the API does work - as you state - the direct register mode (I supplied) provides the higher frequency capability the poster sought...

    cb1_mobile said:

    Here's what we used:  (just showing 1st 4 fnt. calls - we repeated 20+ times to "firm" scope view...)

       while (1)
        {
       
        HWREG(GPIO_PORTF_AHB_BASE + GPIO_O_DATA + (GPIO_PIN_4 << 2)) = GPIO_PIN_4;

        HWREG(GPIO_PORTF_AHB_BASE + GPIO_O_DATA + (GPIO_PIN_4 << 2)) = 0;