Other Parts Discussed in Thread: SW-TM4C
Hello i have recently gotten my hands on the launchpad with the tm4c123g
I am now trying to get the launchpad connected to the PC as a mass storage device using the usblib that i downloaded from here:
http://www.ti.com/tool/sw-tm4c
My (Basic) code looks like this:
// *******************************************************************************************
//
// System clock settings
//
// *******************************************************************************************
// Set clock settings to the default of 12.5Mhz, used crystal is 16 Mhz
uint32_t RCC = (SYSCTL_RCC_XTAL_16MHZ | SYSCTL_RCC_USESYSDIV | (0x15 << SYSCTL_RCC_SYSDIV_S) ); // Oscillator is a 16MhZ crystal, PLL is used so SYSDIV is needed (defaults to 15 for 12.5Mhz clock)
SYSCTL_RCC_R = RCC;
// Override certain register values of the RCC register with the values of the RCC2 register so that we can set the clock speed to 80Mhz
uint32_t RCC2 = (SYSCTL_RCC2_USERCC2 | SYSCTL_RCC2_DIV400 | (2 << SYSCTL_RCC2_SYSDIV2_S) );
SYSCTL_RCC2_R = RCC2;
//***************************************************************
//
// string descriptors for USB
//
//***************************************************************
// language
const uint8_t langDescriptor[] = {
4, // 1st byte gives descriptor length in bytes.
USB_DTYPE_STRING, // Descriptor type
USBShort(USB_LANG_EN_US) // Language code in 2 bytes (0x0409)
};
// Manufacturer
const uint8_t manuDescriptor[] = {
( 7 + 1 ) * 2 , // 1st byte gives descriptor length in bytes.
USB_DTYPE_STRING, // Descriptor type
'A', 0, 'r', 0, 't', 0, 'i', 0, 'n', 0, 'i', 0, 's', 0,
};
// Product
const uint8_t productDescriptor[] = {
( 7 + 1 ) * 2 , // 1st byte gives descriptor length in bytes.
USB_DTYPE_STRING, // Descriptor type
'A', 0, 'r', 0, 't', 0, 'i', 0, 'n', 0, 'i', 0, 's', 0,
};
// Serial number
const uint8_t serialDescriptor[] = {
( 7 + 1 ) * 2 , // 1st byte gives descriptor length in bytes.
USB_DTYPE_STRING, // Descriptor type
'A', 0, 'r', 0, 't', 0, 'i', 0, 'n', 0, 'i', 0, 's', 0,
};
const uint8_t * const stringDescriptors[] = {
langDescriptor,
manuDescriptor,
productDescriptor,
serialDescriptor,
productDescriptor,
productDescriptor
};
tUSBDMSCDevice deviceInfo = {
USB_VID_TI_1CBE, // UID
USB_PID_MSC, // PID
"Artinis ", // Vendor
"PortaProto ", // Product
"0.01", // Revision
500, // Power usage
USB_CONF_ATTR_SELF_PWR, // Power type, bus powered
stringDescriptors, // String descriptors
6,
{
USBDMSCStorageOpen,
USBDMSCStorageClose,
USBDMSCStorageRead,
USBDMSCStorageWrite,
USBDMSCStorageNumBlocks
},
usbEventCallback, // USB callback function
0 // We dont use DMA
};
void* result = USBDMSCInit(0, &deviceInfo);
while(1);
Now when running this code as soon as it enters the main i get these errors in the debug window:
And the device enters the FaultISR(void) routine.
When is remove the tUSBDMSCDevice struct initialization and replace it with the following:
/*tUSBDMSCDevice deviceInfo = {
USB_VID_TI_1CBE, // UID
USB_PID_MSC, // PID
"Artinis ", // Vendor
"PortaProto ", // Product
"0.01", // Revision
500, // Power usage
USB_CONF_ATTR_SELF_PWR, // Power type, bus powered
stringDescriptors, // String descriptors
6,
{
USBDMSCStorageOpen,
USBDMSCStorageClose,
USBDMSCStorageRead,
USBDMSCStorageWrite,
USBDMSCStorageNumBlocks
},
usbEventCallback, // USB callback function
0 // We dont use DMA
};
void *result = USBDMSCInit(0, &deviceInfo);*/
void *result = USBDMSCInit(0, NULL);
The code runs fine! (without usb offcourse)
Can anyone help me with debugging this problem? The code compiles without error or warnings.
Thank you,
Sisco