Other Parts Discussed in Thread: UNIFLASH, TM4C123AH6PM, TM4C1290NCZAD
Hi,
Ive been running into this error code for weeks now:
CORTEX_M4_0: Error connecting to the target: (Error -1063 @ 0x0) Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver. (Emulation package 5.1.232.0)
When attempting to debug a custom board with 3x TM4C123AH5PM processors using CCS Version: 5.5.0.00077 over JTAG with a XDS100v2 debugger. The processors originally would debug to the console using the sample hello world project but all resulted in the same error code once loading a project including the driver libraries.
I ran the debug unlock tool using Uniflash however i'm still no further.
Can anyone help?
Thanks