This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN Pakets Lost

Other Parts Discussed in Thread: TMS570LS3137

Hello,

I am trying to get the CAN Bus of a TMS570LS3137CZWT running properly.

Therefore I've connected two TMS570LS3137 together, where I've wired CAN1 and CAN2 like a crossbar. Now I am sending packet’s with a counting variable and 1 Mbit speed on each controller and check proper reception with the second controller board. I want to know if my CAN driver is working properly.

I’ve noticed that about 0.05% of the packets are dropped (I am not sure at the moment if these packets aren’t sent or aren’t received)

Now I’am in concerned If my CAN System is affected by errata VIM#27.

GCLK is 180 MHz, VCLKA1 is 16MHz , VCLK1 is 90MHz, VCLK2 is 90MHz, VCLK3 is 36MHz

 

Regards,

Lorenz