This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reg Bit banging and I2S interface

Hi Everyone,

I need to interface TM4C123x controller with AIC3254, but the controller don't have digital audio interface, without dual SPI emulation to get I2S, is it possible to do Bit bang to read digital audio data from codec? My customer is using 2 audio codecs, is it possible to connect single audio data reading line to both the codecs like single master and multiple slaves. I will do all the register settings in AIC3254 with the help of control interface, my question is regarding digital audio interface. On the conclusion, i need clarifications on below

1. Is it possible to do bit banging to read digital audio data from codec? If means how to do? Is there any app notes available in web?

2. Like control interface connecting single master control signals to multiple slaves, is it possible for digital audio data transfer also? If means is there any block available in web?

Kindly help me on the above things dear sir/mam.

Regards,

Aravind