Other Parts Discussed in Thread: HALCOGEN
Hi, I am working on RM42x Hercules launchpad. I am falling short of GIO pins and have the following queries.
1. Can SPI , CAN pins be used as GIO pins similar to those of GIOA and HET?
If yes, is there any command similar to that of gioSetBit(Port name, Bit) for SPI and CAN ports?
2. As only 11 pins of HET are physically accessible from the launchpad, how can I use the other 8 pins of HET as output pins? I didn't understand the concept of multiplexing well evn after reading the Technical Ref. Manual.