Other Parts Discussed in Thread: TM4C1294KCPDT, TM4C1294NCPDT
Hi,
I noticed that none the TM4C129x in TQFP-128 package has the LCD Controller circuitry.
Would I be right in assuming that the Graphics library could still be used with the EPI buss once a driver is written?
Also, could you please confirm if these two parts are already in production?
TM4C1294KCPDT (512K flash, TQFP128)
TM4C1294NCPDT (1024K flash, TQFP128)
Thanks.
DJ