Hello everyone,
I am testing the EFUSE self test flow with TMS570LS3137. According to the TRM, the stuck at 0 test should triger ESM3.1 and ESM1.41. I can see these error flags are set. But the error pin in not activated, the register ESMEPSR is 0x1. Does someone also see the same behavior? Or the error pin is only activated for real EFUSE error? I have some other test which activate the error pin. So I am sure the error pin works (the LED at the HDK is on).
Any advice?
Thank you!
Libo