Other Parts Discussed in Thread: TM4C1294NCPDT, EK-TM4C1294XL, TM4C1233H6PZ
HI,
I bought Tiva C Development kit and tried out SPI programming as explained in the spi_master.c file available in the examples folder.
But for some reason all I receive is 0s from the SSI interface. The spi_master program configures SSI in master mode and sends out three letter "s" "p" and "i" and expects them back but all I receive is 0s.
I have my own board which interfaces a spi flash memory with the SSI interface and there also I see the same problem. I do not see the chip select, the SSI0FSS, pin going low and neither I see any clock on the SSI0CLK pin.
Could someone please throw some light on this?
best regards,
Srini